Floating License Help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Floating License Help

Jump to solution
6,383 Views
rdazcal
Contributor III

Greetings,

 

I have one CW "basic" floating licence in my company.

 

When someone is using the license from another computer, I can't even open my CW because the license is in use.

 

But I want to use my CW in the "special (free)" mode. So I have to go and rename the license.dat file to use my local free license. But that is quite uncomfortable.

 

I noticed in the License Manager the following 2 messages when I try to open my CW:

 

1>(metrowks) DENIED: "Win32_CWIDE_Unlimited" Outros@Ticovisc  (Licensed number of users already reached (-4,342))

 

That's fine, license is being used

 

2>(metrowks) UNSUPPORTED: "Win32_CWIDE_Limited" (PORT_AT_HOST_PLUS   ) Outros@Ticovisc  (License server does not support this feature (-18,327))

 

Why is that feature unsupported? Why can't I get the "Win32_CWIDE_Limited" license if the Unlimited is in use?

 

How can I add support for that feature?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
5,557 Views
CrasyCat
Specialist III

Hello

 

You may be missing a line in your license file.

 

Can you send me the content of your client license.dat file as private message?

 

CrasyCat

View solution in original post

0 Kudos
Reply
4 Replies
5,558 Views
CrasyCat
Specialist III

Hello

 

You may be missing a line in your license file.

 

Can you send me the content of your client license.dat file as private message?

 

CrasyCat

0 Kudos
Reply
5,557 Views
Ness
Contributor I

Hi! I am currently using the S12X version of code warrior, but I have the "Win32_CWIDE_Limited" feature missing message when trying to have a license from the licence server, even if the license is available...

 

Any idea?

 

Regards,

 

Nelson.

 

0 Kudos
Reply
5,557 Views
J2MEJediMaster
Specialist I

You might try looking on this licensing FAQ page to see if there is any information on your problem. If that does not help, then I suggest you file a on-service request.

 

---Tom

0 Kudos
Reply
5,557 Views
rdazcal
Contributor III

Thank you CrazyCat

 

That will be a great help!

 

I've sent you the license.dat in a private message

 

Let me know if you haven't got it

0 Kudos
Reply