Flash Programmer Only License

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programmer Only License

ソリューションへジャンプ
6,086件の閲覧回数
pteh
Contributor I

Hi,

 

I'm looking for a (permanent) License to use USB TAP to do Flash Programming only. I don't need any other functionalities of CodeWarrior. Is there such offer in CodeWarrior Licensing or is there other application that offer Flash Programming only via USB TAP? Can someone direct me for more information?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
4,253件の閲覧回数
CrasyCat
Specialist III

Hello

 

You need to purchase a Basic Suite for Code Warrior Power Architectures (Netcomm) Bare Board.

 

According to the description on the CodeWarrior Basic suite at

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-BASIC&tid=CWH

 

For PowerArchitecture BareBoard, a basic suite includes following features:

"

  • Flash Programmer version: Program flash memory on supported devices when used with a CodeWarrior Ethernet or USB TAP.
  • Hardware diagnostics tool (includes memory read/write, memory tests, address test and bus noise test) " 

 

 

CrasyCat

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,253件の閲覧回数
CrasyCat
Specialist III

Hello

 

- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

 

CrasyCat

0 件の賞賛
返信
4,254件の閲覧回数
pteh
Contributor I

Hi,

 

I'm using: CW Dev Studio, Power Architecture, Professional Edition, v8.8, Build 80229 (Evaluation version)

 

I'm targetting PowerQUICC I (8xx), mainly on MPC885.

 

Regards,

 

0 件の賞賛
返信
4,253件の閲覧回数
CrasyCat
Specialist III

Hello

 

You need to purchase a Basic Suite for Code Warrior Power Architectures (Netcomm) Bare Board.

 

According to the description on the CodeWarrior Basic suite at

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-BASIC&tid=CWH

 

For PowerArchitecture BareBoard, a basic suite includes following features:

"

  • Flash Programmer version: Program flash memory on supported devices when used with a CodeWarrior Ethernet or USB TAP.
  • Hardware diagnostics tool (includes memory read/write, memory tests, address test and bus noise test) " 

 

 

CrasyCat

 

0 件の賞賛
返信