Flash Programmer Only License

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programmer Only License

Jump to solution
6,087 Views
pteh
Contributor I

Hi,

 

I'm looking for a (permanent) License to use USB TAP to do Flash Programming only. I don't need any other functionalities of CodeWarrior. Is there such offer in CodeWarrior Licensing or is there other application that offer Flash Programming only via USB TAP? Can someone direct me for more information?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
4,254 Views
CrasyCat
Specialist III

Hello

 

You need to purchase a Basic Suite for Code Warrior Power Architectures (Netcomm) Bare Board.

 

According to the description on the CodeWarrior Basic suite at

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-BASIC&tid=CWH

 

For PowerArchitecture BareBoard, a basic suite includes following features:

"

  • Flash Programmer version: Program flash memory on supported devices when used with a CodeWarrior Ethernet or USB TAP.
  • Hardware diagnostics tool (includes memory read/write, memory tests, address test and bus noise test) " 

 

 

CrasyCat

 

View solution in original post

0 Kudos
Reply
3 Replies
4,254 Views
CrasyCat
Specialist III

Hello

 

- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

 

CrasyCat

0 Kudos
Reply
4,255 Views
pteh
Contributor I

Hi,

 

I'm using: CW Dev Studio, Power Architecture, Professional Edition, v8.8, Build 80229 (Evaluation version)

 

I'm targetting PowerQUICC I (8xx), mainly on MPC885.

 

Regards,

 

0 Kudos
Reply
4,254 Views
CrasyCat
Specialist III

Hello

 

You need to purchase a Basic Suite for Code Warrior Power Architectures (Netcomm) Bare Board.

 

According to the description on the CodeWarrior Basic suite at

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-BASIC&tid=CWH

 

For PowerArchitecture BareBoard, a basic suite includes following features:

"

  • Flash Programmer version: Program flash memory on supported devices when used with a CodeWarrior Ethernet or USB TAP.
  • Hardware diagnostics tool (includes memory read/write, memory tests, address test and bus noise test) " 

 

 

CrasyCat

 

0 Kudos
Reply