Codewarrior Special Edition for PowerPC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Special Edition for PowerPC?

Jump to solution
3,795 Views
emagii
Contributor II

Hi, I installed the CodeWarrior 11.1 in December. This license has now expired.
I have seen that there are (has been) Special Edition versions of this compiler with 128kB limitations.

Since I am working with a bootloader, this is not a problem for me,
but for application developers this will not work
We are not there yet in the decision process however.

What is the latest revision of the Special Edition that supports the MPC5643L?
Can the special edition be downloaded from somewhere?
Can the current evaluation version be extended?

Thanks!

0 Kudos
Reply
1 Solution
3,741 Views
stanish
NXP Employee
NXP Employee

Hi,

CodeWarrior for MCUs v11.x Special edition code size limit is 512kB of C object code for MPC56xx.

You can download Special Edition here:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

But the only difference between version is license file.

So if you install e.g. Evaluation Edition: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1

After the license expires it automatically switches to Special Edition (expired on no license.dat file present).

AFAIK you can extend Evaluation Edition 3 times in total so if you have already evaluated or extended CodeWarrior in past you might already reached this limit.

Hope it helps!

Stan

 

View solution in original post

0 Kudos
Reply
1 Reply
3,742 Views
stanish
NXP Employee
NXP Employee

Hi,

CodeWarrior for MCUs v11.x Special edition code size limit is 512kB of C object code for MPC56xx.

You can download Special Edition here:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

But the only difference between version is license file.

So if you install e.g. Evaluation Edition: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1

After the license expires it automatically switches to Special Edition (expired on no license.dat file present).

AFAIK you can extend Evaluation Edition 3 times in total so if you have already evaluated or extended CodeWarrior in past you might already reached this limit.

Hope it helps!

Stan

 

0 Kudos
Reply