Codewarrior Special Edition for PowerPC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Special Edition for PowerPC?

ソリューションへジャンプ
3,795件の閲覧回数
emagii
Contributor II

Hi, I installed the CodeWarrior 11.1 in December. This license has now expired.
I have seen that there are (has been) Special Edition versions of this compiler with 128kB limitations.

Since I am working with a bootloader, this is not a problem for me,
but for application developers this will not work
We are not there yet in the decision process however.

What is the latest revision of the Special Edition that supports the MPC5643L?
Can the special edition be downloaded from somewhere?
Can the current evaluation version be extended?

Thanks!

0 件の賞賛
返信
1 解決策
3,741件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

CodeWarrior for MCUs v11.x Special edition code size limit is 512kB of C object code for MPC56xx.

You can download Special Edition here:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

But the only difference between version is license file.

So if you install e.g. Evaluation Edition: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1

After the license expires it automatically switches to Special Edition (expired on no license.dat file present).

AFAIK you can extend Evaluation Edition 3 times in total so if you have already evaluated or extended CodeWarrior in past you might already reached this limit.

Hope it helps!

Stan

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,742件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

CodeWarrior for MCUs v11.x Special edition code size limit is 512kB of C object code for MPC56xx.

You can download Special Edition here:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

But the only difference between version is license file.

So if you install e.g. Evaluation Edition: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1

After the license expires it automatically switches to Special Edition (expired on no license.dat file present).

AFAIK you can extend Evaluation Edition 3 times in total so if you have already evaluated or extended CodeWarrior in past you might already reached this limit.

Hope it helps!

Stan

 

0 件の賞賛
返信