CodeWarrior mac os x lion [intel]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior mac os x lion [intel]

跳至解决方案
8,737 次查看
marcoarigliani
Contributor I

hi.

I'm a student of a school of electronics in Italy.

in my school we are learning to program for freescale microcontrollers, and we use the USBDM.

the problem is that I am a mac user.

I downloaded a version from this site -->CodeWarrior for MAC OS

but there are only versions for power pc.

I need a version for intel.

I apologize if you did not understand.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,343 次查看
CrasyCat
Specialist III

Hello

Freescale do not provide CodeWarrior for MCU hosted on MAC.

The list of the supported hosts for CodeWarrior for Microcontroller is available at following URL:

    CodeWarrior for MCUs (Eclipse IDE) - RS08/HCS08, ColdFire V1, Qorivva 56xx, PX Series, 56800/E DSC, ...

If you have to stick with a MAC OS as host the only think you can try out is use a virtual machine to run Windows XP and CodeWarrior and write code that way. Search the forum a bit. As far as I remember we have other customers who manage to work that way.

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,344 次查看
CrasyCat
Specialist III

Hello

Freescale do not provide CodeWarrior for MCU hosted on MAC.

The list of the supported hosts for CodeWarrior for Microcontroller is available at following URL:

    CodeWarrior for MCUs (Eclipse IDE) - RS08/HCS08, ColdFire V1, Qorivva 56xx, PX Series, 56800/E DSC, ...

If you have to stick with a MAC OS as host the only think you can try out is use a virtual machine to run Windows XP and CodeWarrior and write code that way. Search the forum a bit. As far as I remember we have other customers who manage to work that way.

CrasyCat

0 项奖励
回复