CodeWarrior mac os x lion [intel]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior mac os x lion [intel]

Jump to solution
9,620 Views
marcoarigliani
Contributor I

hi.

I'm a student of a school of electronics in Italy.

in my school we are learning to program for freescale microcontrollers, and we use the USBDM.

the problem is that I am a mac user.

I downloaded a version from this site -->CodeWarrior for MAC OS

but there are only versions for power pc.

I need a version for intel.

I apologize if you did not understand.

Labels (1)
0 Kudos
Reply
1 Solution
3,226 Views
CrasyCat
Specialist III

Hello

Freescale do not provide CodeWarrior for MCU hosted on MAC.

The list of the supported hosts for CodeWarrior for Microcontroller is available at following URL:

    CodeWarrior for MCUs (Eclipse IDE) - RS08/HCS08, ColdFire V1, Qorivva 56xx, PX Series, 56800/E DSC, ...

If you have to stick with a MAC OS as host the only think you can try out is use a virtual machine to run Windows XP and CodeWarrior and write code that way. Search the forum a bit. As far as I remember we have other customers who manage to work that way.

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
3,227 Views
CrasyCat
Specialist III

Hello

Freescale do not provide CodeWarrior for MCU hosted on MAC.

The list of the supported hosts for CodeWarrior for Microcontroller is available at following URL:

    CodeWarrior for MCUs (Eclipse IDE) - RS08/HCS08, ColdFire V1, Qorivva 56xx, PX Series, 56800/E DSC, ...

If you have to stick with a MAC OS as host the only think you can try out is use a virtual machine to run Windows XP and CodeWarrior and write code that way. Search the forum a bit. As far as I remember we have other customers who manage to work that way.

CrasyCat

0 Kudos
Reply