CodeWarrior for MPC5xx IDE installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for MPC5xx IDE installation

ソリューションへジャンプ
6,126件の閲覧回数
zhaoqinsu
NXP Employee
NXP Employee

When I install the CodeWarrior 8.7, a warning appears as shown in the attachment image. How do i choose? How can this software be registered? If the license expired, and how to do it?

0 件の賞賛
返信
1 解決策
5,508件の閲覧回数
stanish
NXP Employee
NXP Employee

Could you possibly try to experiment with windows compatibility mode?

pastedImage_3.png

Anyway I'm afraid if it does not help my only recommendation is to install this old version into a Win XP 32 bit virtual machine (VirtualBox, VM Ware, Virtual PC...)

Stan

元の投稿で解決策を見る

6 返答(返信)
5,508件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

this is pretty old version of CodeWarrior for MPC5xx v8.7.

This version has never been tested on Windows 7+ therefore you might face problems when trying to install it.

You might experiment with both options to figure out which one leads to complete installation.

Note:

If you debug using PEMicro P&E probe you can try to install updated drivers that should supports Windows 7, 8, 10 

http://www.pemicro.com/downloads/download_file.cfm?download_id=53 

The evaluation license is included in evaluation edition installer:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MPC-5XX-EX 

You can access it via your nxp.com account:

pastedImage_3.png

Hope it helps.

Stan

0 件の賞賛
返信
5,508件の閲覧回数
zhaoqinsu
NXP Employee
NXP Employee

Hello Sliva ,

I can give you  one picture of my installing Codewarrior when it comes error ,Can you give me some advice installing Codewarrior?Untitled.png

0 件の賞賛
返信
5,508件の閲覧回数
stanish
NXP Employee
NXP Employee

Could you possibly try to experiment with windows compatibility mode?

pastedImage_3.png

Anyway I'm afraid if it does not help my only recommendation is to install this old version into a Win XP 32 bit virtual machine (VirtualBox, VM Ware, Virtual PC...)

Stan

5,508件の閲覧回数
zhaoqinsu
NXP Employee
NXP Employee

 Thanks for your help ,Codewarrior works well now . But it can't open suffix ".mcp " project .Have you ever met this situation?

picture2.png

5,508件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Could you make sure the project you are trying to open is indeed intended for the version of CW for MPC5xx ?

S32K14x sounds to me like an arm based rather then MPC5xx.

S.

5,508件の閲覧回数
zhaoqinsu
NXP Employee
NXP Employee

Yes , it is indeed intended for the version of CW for MPC5xx.

The  project has run on other guys' Codewarrior.

Important to note, we are using the exact same versions of codewarrior and I am able to open and work with other codewarrior projects

0 件の賞賛
返信