CodeWarrior USB Dongle Licensing error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior USB Dongle Licensing error

4,269 次查看
elel
Contributor III

Hallo,

I'm having a problem with my CodeWarrior 7.2 license. When I try to open the CodeWarrior this error shows up.

 

175133_175133.pngCwError.png

 

We purchased the USB dongle and the perpetual license on 14/07/2014 and I have used it without problems since july 2016. After that I didn't open it until today when I found the error above. These are the license details taken from the invoice (from www.digikey.com):

 

CWP-BASIC-NL-ND
SOFTWARE CW BASIC PERP NODE LOCK
HTSUS: 8523.49.4000 ECCN: EAR99
LEAD: LEAD NA ROHS: ROHS NA
COUNTRY/ORIGIN: MALAYSIA
CAGE: 04713

 

CWH-DONGLE-ND
KIT USB DONGLE DEVICE
HTSUS: 8473.30.1180 ECCN: EAR99
LEAD: LEAD FREE ROHS: ROHS COMP
COUNTRY/ORIGIN: MALAYSIA
CAGE: 04713

 

I attach the license file I have.

 

Thanks in advance.

 

Best regards,

Gianluca Falavigna

Elco Elettronica

Original Attachment has been moved to: license.dat.zip

标签 (1)
0 项奖励
回复
2 回复数

3,302 次查看
stanish
NXP Employee
NXP Employee

Hi 

You are using dongle node-locked license. Can you please check if your dongle FLEXID is visible by LMTOOLS?

Does the FLEXID matches with ID printed on the USB Key and with FLEXID in the license.dat?

pastedImage_2.png

pastedImage_3.png

0 项奖励
回复

3,300 次查看
stanish
NXP Employee
NXP Employee

Note: If all FlexIDs match and you still cannot start CodeWarrior please try to install attached alternative USB dongle drivers.

Please follow the instructions below:

1) unplug the USB dongle 
2) run FLEXid Clean Utility (USB Dongle Drivers|NXP )
3) extract the attached ZIP archive 
4) run the Click_To_Install_Drivers.bat file.
5) Reboot machine
6) attach the USB Dongle and run CodeWarrior

Hope it helps.

Stan

0 项奖励
回复