CodeWarrior Floating License Not working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Floating License Not working?

ソリューションへジャンプ
3,018件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    We bought a CodeWarrior Floating License.But It is not working.We followed the Documentation provided by freescale but still it is not able to connect to the server.

 

I have attached the Documentation and Screenshhot of Server Stattus and Server Diagnostics in the .zip file.

 

I am not able to connect to the server.I am actually using the same Machine as Server and Client.Eventhough I have tried pinging the server and I got a response for it.

Original Attachment has been moved to: codewarriorlicensenotworking.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
2,455件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

Share the license server heather

Review if you have added the license file on both side, the application for example

On C:\Freescale\CW MCU v10.6\MCU

And also on the location specified on the license manager

  pastedImage_1.png

If you are using the same station as client and server, make sure you use the correct client name and the Ethernet MAC address or Disk Serial

  pastedImage_2.png

I expect to see something similar on your license.dat

SERVER b33911-12 ECF4BB52F0AA

VENDOR metrowks

USE_SERVER

Check the new guide , you are using a previous version, check this link

https://cache.nxp.com/files/soft_dev_tools/doc/quick_ref_guide/SWSUPPACTQS.pdf

https://cache.nxp.com/files/soft_dev_tools/doc/brochure/FLTLICINSTWINBR.pdf

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,456件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

Share the license server heather

Review if you have added the license file on both side, the application for example

On C:\Freescale\CW MCU v10.6\MCU

And also on the location specified on the license manager

  pastedImage_1.png

If you are using the same station as client and server, make sure you use the correct client name and the Ethernet MAC address or Disk Serial

  pastedImage_2.png

I expect to see something similar on your license.dat

SERVER b33911-12 ECF4BB52F0AA

VENDOR metrowks

USE_SERVER

Check the new guide , you are using a previous version, check this link

https://cache.nxp.com/files/soft_dev_tools/doc/quick_ref_guide/SWSUPPACTQS.pdf

https://cache.nxp.com/files/soft_dev_tools/doc/brochure/FLTLICINSTWINBR.pdf

0 件の賞賛
返信