Client computer not able to obtain CW license from the Server

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Client computer not able to obtain CW license from the Server

跳至解决方案
2,975 次查看
rhagberg
Contributor I

I have set up a floating license for Code Warrior on our license server at work, and it seems to be up and running. When I start Code Warrior it tries to obtain a license from the server, but never get's a response. I have used wire shark on both the client and the server and can see the request going to the server, but the server never responds.  I have set up the firewall on the server to allow TCP and UDP from the client to pass through, and still no response. Eventually Code Warrior times out and gives me the following error messages. I would appreciate any help as I am unsure of what to try next. Thank you.

CWLicenseErrors.PNG

0 项奖励
回复
1 解答
2,900 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you help me perform the steps below:

 

Server Side:

  1. Can you send me the logs
  2. Open a CMD and go to the location where theFlexLM is hosted
  3. Run the command lmgrd -z
  4. Please send me a screen capture of the result

Client Side:

  1. open a CMD and do a telnet to the server with the port number eg. 128.0.0.0  2700
    1. send me a screen capture of the result

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,901 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you help me perform the steps below:

 

Server Side:

  1. Can you send me the logs
  2. Open a CMD and go to the location where theFlexLM is hosted
  3. Run the command lmgrd -z
  4. Please send me a screen capture of the result

Client Side:

  1. open a CMD and do a telnet to the server with the port number eg. 128.0.0.0  2700
    1. send me a screen capture of the result
0 项奖励
回复