CW10.7 License time limit problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.7 License time limit problem

ソリューションへジャンプ
1,770件の閲覧回数
peterpanda
Contributor I

I am using a free code to restrict the version,Why is there a license time limit?I use the version is  Special Edition: CodeWarrior® for Microcontrollers 10.7 (Eclipse, Offline)(REV 10.7)

11.JPG

タグ(1)
1 解決策
1,532件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Peter,

You probably installed a CodeWarrior Evaluation version of the installer which basically includes 30 day full feature license (Professional Edition). As soon as this evaluation period expires the license should automatically switch to Special Edition - permanent but feature limited.

You can do a quick check to confirm my hypothesis - check if the license.dat file exists here:

c:\Freescale\CW MCU v10.7\MCU\license.dat

No license = Special Edition

License.dat = Evaluation Edition

Hope it helps.

Stan

元の投稿で解決策を見る

1 返信
1,533件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Peter,

You probably installed a CodeWarrior Evaluation version of the installer which basically includes 30 day full feature license (Professional Edition). As soon as this evaluation period expires the license should automatically switch to Special Edition - permanent but feature limited.

You can do a quick check to confirm my hypothesis - check if the license.dat file exists here:

c:\Freescale\CW MCU v10.7\MCU\license.dat

No license = Special Edition

License.dat = Evaluation Edition

Hope it helps.

Stan