CW10.7 License time limit problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.7 License time limit problem

Jump to solution
1,784 Views
peterpanda
Contributor I

I am using a free code to restrict the version,Why is there a license time limit?I use the version is  Special Edition: CodeWarrior® for Microcontrollers 10.7 (Eclipse, Offline)(REV 10.7)

11.JPG

Tags (1)
1 Solution
1,546 Views
stanish
NXP Employee
NXP Employee

Hello Peter,

You probably installed a CodeWarrior Evaluation version of the installer which basically includes 30 day full feature license (Professional Edition). As soon as this evaluation period expires the license should automatically switch to Special Edition - permanent but feature limited.

You can do a quick check to confirm my hypothesis - check if the license.dat file exists here:

c:\Freescale\CW MCU v10.7\MCU\license.dat

No license = Special Edition

License.dat = Evaluation Edition

Hope it helps.

Stan

View solution in original post

1 Reply
1,547 Views
stanish
NXP Employee
NXP Employee

Hello Peter,

You probably installed a CodeWarrior Evaluation version of the installer which basically includes 30 day full feature license (Professional Edition). As soon as this evaluation period expires the license should automatically switch to Special Edition - permanent but feature limited.

You can do a quick check to confirm my hypothesis - check if the license.dat file exists here:

c:\Freescale\CW MCU v10.7\MCU\license.dat

No license = Special Edition

License.dat = Evaluation Edition

Hope it helps.

Stan