30-day evaluation license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

30-day evaluation license

Jump to solution
10,378 Views
Smay
Contributor I
Hello,
I downloaded an evaluation copy of Codewarrior HC12 V4.6 to test it with a MC9S12NE64 microprocessor. I would like to obtain a 30-day evaluation license and sent a mail to l[email protected] as discribed in the download menu. Unfortunately I haven´t received a response yet :smileysad:
 
Do I have to send some special information (i.e. about the project) or did something else wrong?
 
Thanks,
Stefan May
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
7,691 Views
Alban
Senior Contributor II
Hello Wayne,
 
Add this line in your license.dat file:
 
Code:
FEATURE PE_Advanced_BeansHCS12 metrowks 1.000 1-apr-2007 uncounted \ 253ADD6B8B01 VENDOR_STRING=163E94D42D01E5E171C0105CC88049C5 \ HOSTID=ANY ck=97

 
Expiration date is 1st April = 1 month.
 
Alban.

View solution in original post

0 Kudos
Reply
10 Replies
7,691 Views
WayneHowell
Contributor I
Hello,
 
I'm going mad fighting with license files. Anyone please help!
 
After much pain I know have V4.6 Codewarrior prof version installed. I have a 30 day license installed which has removed the file number and code size limit.
 
The problem is that I'm using advanced beans in the processor expert (Ethernet). When I compile, an error message informs me my license does not allow advanced beans.
 
But tech support in the UK and the freescale web site confirm that the 30 day prof license should allow this.
 
Help .....
 
Wayne Howell
0 Kudos
Reply
7,691 Views
Smay
Contributor I
Got the license file today.
Thanks alot :smileyhappy:
 
Stefan May
0 Kudos
Reply
7,691 Views
Alban
Senior Contributor II
Hello Wayne,
 
When updating the license.dat, I always append the information and not remove the previous content.
If you could indicate the ERROR Code that could help us giving you the right line for the license.
 
Cheers,
Alban.
0 Kudos
Reply
7,691 Views
WayneHowell
Contributor I
Hi there,
 
The error is displayed when I load the project. Code is -5,357. Message "Processor Expertlicense 'Advanced Beans' for HCS12 family was not found or is not valid".
 
Flexlm detailed info:
 
No such feature exists.
Feature PE_Advanced_BeansHCS12
 
 
Hope you can help.
 
Thanks
 
Wayne
0 Kudos
Reply
7,691 Views
WayneHowell
Contributor I
Hi,
 
More info:
 
The Bean wizard also causes the same error code and then locks up Code Warrior.
 
Thanks
 
Wayne
0 Kudos
Reply
7,692 Views
Alban
Senior Contributor II
Hello Wayne,
 
Add this line in your license.dat file:
 
Code:
FEATURE PE_Advanced_BeansHCS12 metrowks 1.000 1-apr-2007 uncounted \ 253ADD6B8B01 VENDOR_STRING=163E94D42D01E5E171C0105CC88049C5 \ HOSTID=ANY ck=97

 
Expiration date is 1st April = 1 month.
 
Alban.
0 Kudos
Reply
7,691 Views
WayneHowell
Contributor I
Hi Alban,
 
Many thanks that has got the advanced bean working.
 
Unfortunately the Bean Wizard is still not working, although it no longer crashes.
 
The error code is: -5,357.
 
Thanks.
 
Wayne
0 Kudos
Reply
7,691 Views
Alban
Senior Contributor II
Hello,
 
Please send me your email address via Private Message so we can fix that. Not on the board.
 
Cheers,
Alban.
0 Kudos
Reply
7,690 Views
WayneHowell
Contributor I
0 Kudos
Reply
7,690 Views
Alban
Senior Contributor II
Hello Stefan
 
I believe the information you are looking for is in the link:
 
Cheers,
Alban.
0 Kudos
Reply