RSA does not work with SE050E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RSA does not work with SE050E

ソリューションへジャンプ
2,775件の閲覧回数
anna_geber
Contributor I

Hello, I am currently unable to use the RSA asymmetric encryption method with my SE050E. Is this due to the hardware? Or is it due to the software settings? As shown in document AN13483 (see attachment), "RSA_PLAIN" and "RSA_CRT" are also set to "WithOut" for me. Is it possible to set "RSA_PLAIN" and "RSA_CRT" to "With"?

#https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trus...

ラベル(1)
0 件の賞賛
返信
1 解決策
2,763件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,764件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信