RSA does not work with SE050E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RSA does not work with SE050E

跳至解决方案
2,761 次查看
anna_geber
Contributor I

Hello, I am currently unable to use the RSA asymmetric encryption method with my SE050E. Is this due to the hardware? Or is it due to the software settings? As shown in document AN13483 (see attachment), "RSA_PLAIN" and "RSA_CRT" are also set to "WithOut" for me. Is it possible to set "RSA_PLAIN" and "RSA_CRT" to "With"?

#https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trus...

标签 (1)
0 项奖励
回复
1 解答
2,749 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,750 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复