RSA does not work with SE050E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RSA does not work with SE050E

Jump to solution
2,707 Views
anna_geber
Contributor I

Hello, I am currently unable to use the RSA asymmetric encryption method with my SE050E. Is this due to the hardware? Or is it due to the software settings? As shown in document AN13483 (see attachment), "RSA_PLAIN" and "RSA_CRT" are also set to "WithOut" for me. Is it possible to set "RSA_PLAIN" and "RSA_CRT" to "With"?

#https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trus...

Labels (1)
0 Kudos
Reply
1 Solution
2,695 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,696 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @anna_geber ,

 

Actually SE050E doesn't support RSA indeed, please use SE050F2 instead. please refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply