how to use Pressure Measurement Characteristic to calculate Pressure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use Pressure Measurement Characteristic to calculate Pressure

2,043 次查看
javierpernia
Contributor I

hi, I'm working in a project with TPMS. using the example program i get de array gu16UUAA, looking at the formula i dont know how to calculate de pressure using that table. please any guide will be appreciated

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,813 次查看
darioarias
NXP Employee
NXP Employee

Hi Javier,

You only need to substitute the values in this transfer function.

P = ΔP1500 x PCODE + (100 – ΔP1500)

Example:

ΔP1500 = 2.750 kPa/count (Should be in the datasheet on pressure measurement characteristics)

PCODE = 0x20 = 32

P = 2.750 kpa/count x 32 count + (100 - 2.750 kPa/count)

P = 88 kPa + 97.25 kpa

P = 185.25 kPa

You can also refer to the attachment for more detail in the correspondence between compensated data in common units.

Regards,

Darío

0 项奖励
回复