how to add the support of the gdbserver on the S32Rxx devices using Yocto to add that packages?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to add the support of the gdbserver on the S32Rxx devices using Yocto to add that packages?

Jump to solution
1,190 Views
sinetech
Contributor II

Hi, 

how to add the support of the gdbserver on the S32Rxx devices using Yocto to add that packages?

 

Regard,

ray.

0 Kudos
Reply
1 Solution
1,071 Views
junzhu-b40054
NXP Employee
NXP Employee

Confirmed with Sinetech, gdb server can work now, close the ticket.

View solution in original post

0 Kudos
Reply
2 Replies
1,072 Views
junzhu-b40054
NXP Employee
NXP Employee

Confirmed with Sinetech, gdb server can work now, close the ticket.

0 Kudos
Reply
1,157 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not sure here. Let me talk to RADAR team and I will feedback you ASAP.

Best regards,

Peter

0 Kudos
Reply