freescale 9-axis sensor fusion specification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

freescale 9-axis sensor fusion specification

跳至解决方案
4,717 次查看
kyleyang
Contributor IV

Hi

 

There is a customer survey 9-axis fusion for UAV and indoor navigation, but they have no experience before.

They have study other UAV product and list a specification table.

But there are some information that I can not find in datasheet.

Can anybody help provide some information to help fill this table?

I want to design in and win this case.

Really appreciate your help.

 

Customerfreescale
Gyro SpecificationsRange±2000 °/s±2000 °/sFXAS21002
In-Run Bias Stability< 10 °/hr
Linearity< 0.1 % FS±0.5 %FSR
Noise Density0.0035 °/s / Hz0.025 dps/√Hz
Bandwidth256 Hz256 Hz
Alignment Error±0.05 °
Accelerometer SpecificationsRange±16 g±8FXOS8700
In-Run Bias Stability< 0.04 mg
Linearity< 0.5 % FS±0.5 %FS
Noise Density0.14 mg/ Hz<126 μg/√Hz
Bandwidth260 Hz200 Hz
Alignment Error±0.05 °
Magnetometer SpecificationsRange±2.5 Gauss±1200 uTFXOS8700
Linearity< 0.1 %±1 % %FS
Noise Density140 μGauss/ Hz< 100 nT/√Hz
Bandwidth200 Hz200 Hz
Alignment Error±0.05 °
Pressure Sensor SpecificationsRange10 to 1200 mbar50 to 110 kPaMPL3115
Resolution0.042 mbar1.5 Pa
Accuracy±1.5 mbar±0.4 kPa
Error Band±2.5 mbar
Bandwidth200 Hz
Attitude & HeadingRange (Heading/Roll)±180 °±180 °
Range (Pitch)±90 °±90 °
"Static Accuracy
(Heading, Magnetic)"2.0 ° RMS1.21° RMS
"Static Accuracy
(Pitch/Roll)"0.5 ° RMS1.21° RMS
"Dynamic Accuracy
(Heading, Magnetic)"2.0 ° RMS1.06° RMS
"Dynamic Accuracy
(Pitch/Roll)"1.0 ° RMS1.06° RMS
Angular Resolution< 0.05 °
Repeatability< 0.2°
Output Rate (IMU Data)1 kHz
Output Rate (Attitude Data)400 Hz
Individually calibrated for bias, scalefactor, misalignment, & gyro g-sensitivityReal-time magnetic & acceleration disturbance rejectionSupport
Adaptive signal filteringSupport
Dynamic filter tuningSupport
On-board Hard & Soft Iron compensationSupportSupport
On-board gyro drift compensationSupport
标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,950 次查看
michaelestanley
NXP Employee
NXP Employee

Kyle,

Great start on a spec.  I would like to set up a phone call to get a better idea of your opportunity and how Freescale can help.  In the meantime, I'm routing your spreadsheet to my team to see what additional information we can add.

Could you send me your contact details via email to Mike.Stanley@Freescale.com?

Thanks!

Miek

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,951 次查看
michaelestanley
NXP Employee
NXP Employee

Kyle,

Great start on a spec.  I would like to set up a phone call to get a better idea of your opportunity and how Freescale can help.  In the meantime, I'm routing your spreadsheet to my team to see what additional information we can add.

Could you send me your contact details via email to Mike.Stanley@Freescale.com?

Thanks!

Miek

0 项奖励
回复
3,911 次查看
Bilgin
Contributor I

Hi Mike

I get a 13 degree sensor output on a 13.7 degree surface. It says there is an ancestor of 0.05 degrees per degree according to this table

Is the accelerometer alignment error in the table per degree ? I hope I'm not wrong

0 项奖励
回复
3,950 次查看
kyleyang
Contributor IV

Hi Mike

Appreciate your help.

0 项奖励
回复