freescale 9-axis sensor fusion specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

freescale 9-axis sensor fusion specification

ソリューションへジャンプ
4,680件の閲覧回数
kyleyang
Contributor IV

Hi

 

There is a customer survey 9-axis fusion for UAV and indoor navigation, but they have no experience before.

They have study other UAV product and list a specification table.

But there are some information that I can not find in datasheet.

Can anybody help provide some information to help fill this table?

I want to design in and win this case.

Really appreciate your help.

 

Customerfreescale
Gyro SpecificationsRange±2000 °/s±2000 °/sFXAS21002
In-Run Bias Stability< 10 °/hr
Linearity< 0.1 % FS±0.5 %FSR
Noise Density0.0035 °/s / Hz0.025 dps/√Hz
Bandwidth256 Hz256 Hz
Alignment Error±0.05 °
Accelerometer SpecificationsRange±16 g±8FXOS8700
In-Run Bias Stability< 0.04 mg
Linearity< 0.5 % FS±0.5 %FS
Noise Density0.14 mg/ Hz<126 μg/√Hz
Bandwidth260 Hz200 Hz
Alignment Error±0.05 °
Magnetometer SpecificationsRange±2.5 Gauss±1200 uTFXOS8700
Linearity< 0.1 %±1 % %FS
Noise Density140 μGauss/ Hz< 100 nT/√Hz
Bandwidth200 Hz200 Hz
Alignment Error±0.05 °
Pressure Sensor SpecificationsRange10 to 1200 mbar50 to 110 kPaMPL3115
Resolution0.042 mbar1.5 Pa
Accuracy±1.5 mbar±0.4 kPa
Error Band±2.5 mbar
Bandwidth200 Hz
Attitude & HeadingRange (Heading/Roll)±180 °±180 °
Range (Pitch)±90 °±90 °
"Static Accuracy
(Heading, Magnetic)"2.0 ° RMS1.21° RMS
"Static Accuracy
(Pitch/Roll)"0.5 ° RMS1.21° RMS
"Dynamic Accuracy
(Heading, Magnetic)"2.0 ° RMS1.06° RMS
"Dynamic Accuracy
(Pitch/Roll)"1.0 ° RMS1.06° RMS
Angular Resolution< 0.05 °
Repeatability< 0.2°
Output Rate (IMU Data)1 kHz
Output Rate (Attitude Data)400 Hz
Individually calibrated for bias, scalefactor, misalignment, & gyro g-sensitivityReal-time magnetic & acceleration disturbance rejectionSupport
Adaptive signal filteringSupport
Dynamic filter tuningSupport
On-board Hard & Soft Iron compensationSupportSupport
On-board gyro drift compensationSupport
ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,913件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Kyle,

Great start on a spec.  I would like to set up a phone call to get a better idea of your opportunity and how Freescale can help.  In the meantime, I'm routing your spreadsheet to my team to see what additional information we can add.

Could you send me your contact details via email to Mike.Stanley@Freescale.com?

Thanks!

Miek

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,914件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Kyle,

Great start on a spec.  I would like to set up a phone call to get a better idea of your opportunity and how Freescale can help.  In the meantime, I'm routing your spreadsheet to my team to see what additional information we can add.

Could you send me your contact details via email to Mike.Stanley@Freescale.com?

Thanks!

Miek

0 件の賞賛
返信
3,874件の閲覧回数
Bilgin
Contributor I

Hi Mike

I get a 13 degree sensor output on a 13.7 degree surface. It says there is an ancestor of 0.05 degrees per degree according to this table

Is the accelerometer alignment error in the table per degree ? I hope I'm not wrong

0 件の賞賛
返信
3,913件の閲覧回数
kyleyang
Contributor IV

Hi Mike

Appreciate your help.

0 件の賞賛
返信