accelerometer with interrupt on relative change in acceleration (not change relative to a constant accelleration)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

accelerometer with interrupt on relative change in acceleration (not change relative to a constant accelleration)?

1,124件の閲覧回数
tedhuntington
Contributor I

Are there any low-g XYZ Accelerators that can send an interrupt on relative change in acceleration (not absolute acceleration)? This is more useful to me than the freefall or motion detection of interrupt, for example in the MMA8652, which just compares the acceleration to a constant value.

ラベル(1)
0 件の賞賛
返信
1 返信

917件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ted,

Yes, we do have the FXLS8471Q accelerometer with an embedded vector-magnitude function that can be configured to generate an interrupt when the acceleration magnitude exceeds a preset threshold for a programmed debounce time. This function can be configured to operate in absolute or relative modes and can also act as a wake to sleep/sleep to wake source. For more information please refer to the AN4692.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信