Terminal finish, ESD and MSL Level for MPXM2202A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Terminal finish, ESD and MSL Level for MPXM2202A

ソリューションへジャンプ
2,361件の閲覧回数
cesarmuniz
Contributor I

Hello to all.  Trying to figure out the following information ofMPXM2202A:

  1. Terminal finish
  2. ESD level
  3. MSL level

Appreciate the help.

TryinTryindfadfdfsfwsds

ラベル(1)
0 件の賞賛
返信
1 解決策
1,763件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Cesar,

1. Terminal Finish:

Plating on the leads is NiPdAu.

2. ESD Level:

NXP Pressure sensors are Class 1 ESD, so it has a range up to 2000 Volts (ESD).

Electrostatic Discharge will applied according Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts.

3. MSL Level:

MSL = n/a because it is an open cavity device.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,764件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Cesar,

1. Terminal Finish:

Plating on the leads is NiPdAu.

2. ESD Level:

NXP Pressure sensors are Class 1 ESD, so it has a range up to 2000 Volts (ESD).

Electrostatic Discharge will applied according Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts.

3. MSL Level:

MSL = n/a because it is an open cavity device.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信