Terminal finish, ESD and MSL Level for MPXM2202A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Terminal finish, ESD and MSL Level for MPXM2202A

Jump to solution
2,364 Views
cesarmuniz
Contributor I

Hello to all.  Trying to figure out the following information ofMPXM2202A:

  1. Terminal finish
  2. ESD level
  3. MSL level

Appreciate the help.

TryinTryindfadfdfsfwsds

Labels (1)
0 Kudos
Reply
1 Solution
1,766 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Cesar,

1. Terminal Finish:

Plating on the leads is NiPdAu.

2. ESD Level:

NXP Pressure sensors are Class 1 ESD, so it has a range up to 2000 Volts (ESD).

Electrostatic Discharge will applied according Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts.

3. MSL Level:

MSL = n/a because it is an open cavity device.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,767 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Cesar,

1. Terminal Finish:

Plating on the leads is NiPdAu.

2. ESD Level:

NXP Pressure sensors are Class 1 ESD, so it has a range up to 2000 Volts (ESD).

Electrostatic Discharge will applied according Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts.

3. MSL Level:

MSL = n/a because it is an open cavity device.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply