TPMS Sensors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,279件の閲覧回数
lalit0611
Contributor II

Hi,

I am very new to TPMS sensors, I just read about them and though that it would be cool to fit them in my car.So I was looking at FXTH87 sensors, but I could not figure out how the sensor is going to read the tyre pressure and where will it be fit on the wheel? Also I looked at the FXTH87 Evaluation Manual, it said that a BDM Multilink is required to program the chip, but it appears that is being discontinued and will be taken over by UMultiLink, but I couldn't find the FXTH87 name under the supported micro-controllers. Can someone clarify on that too?

Thanks in advance for the help :smileyhappy:

ラベル(1)
タグ(2)
1 解決策
3,664件の閲覧回数
sushilnikam
Contributor III

HI Lalit,

Basically there are two methods of mounting the sensor

1. Inside the tyre

2. Outside the tyre means on the valve of the tyre.

For example if you put the sensor on the valve (outside the tyre) it has to push the valve so that the AIr Pressure will be force on the TPMS chip. As the TPMS application chip is having on chip pressure sensor it will sense the pressure and provide you the corresponding data. To understand the complete system you have to study the Internal Architecture of it. Its very difficult for me to tell you whole thing here.

Thanks & Regards

Sushil

元の投稿で解決策を見る

7 返答(返信)
3,664件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello,

First of all, please refer to the Tire Pressure Monitoring System (TPMS) main web page in order to get more information, recommended products, demos and documentation, at:

Tire Pressure Monitoring System (TPMS)|Freescale

With regard to your first questions, I would like to recommend the following document:

A Global Solution for Tire Pressure Monitoring System

The document mentioned addresses the requirements of tire pressure monitoring systems and variations in implementing them as well as the latest technology for a system-in-package solution and a discussion about advancements that could occur in the near future.

Regarding your last question, The FXTH87 has an S08, 8-bit microprocessor core, therefore you would require a universal BDM and CodeWarrior to program it.

I would recommend you the following BDM interface:

Universal Multilink Development Interface|Freescale

I hope all this information will be useful for you. In case you still have questions or you need me to be more specific, please let me know. I will be glad to help.

Have an excellent day :smileyhappy:

David

3,664件の閲覧回数
lalit0611
Contributor II

Your post answers most of my questions. But I'm unable to figure out where on tyre will TPMS be mounted and how does it measure the pressure? Does it work like those manual pressure gauge, where you put the device over tyre valve and let some air out to check the pressure or something different. Sorry if it's a silly question but I'm unable to imagine how it'll fit over the tyre :smileysad:

0 件の賞賛
返信
3,664件の閲覧回数
timgillman
Contributor I

If you look on the block diagram on the page previously mentioned, you will see that it uses RF communications. The sensors go inside the tires : Tire Pressure Monitoring System (TPMS)|Freescale

0 件の賞賛
返信
3,665件の閲覧回数
sushilnikam
Contributor III

HI Lalit,

Basically there are two methods of mounting the sensor

1. Inside the tyre

2. Outside the tyre means on the valve of the tyre.

For example if you put the sensor on the valve (outside the tyre) it has to push the valve so that the AIr Pressure will be force on the TPMS chip. As the TPMS application chip is having on chip pressure sensor it will sense the pressure and provide you the corresponding data. To understand the complete system you have to study the Internal Architecture of it. Its very difficult for me to tell you whole thing here.

Thanks & Regards

Sushil

3,664件の閲覧回数
lalit0611
Contributor II

One last doubt (in this post :smileysilly: ), is this the right version of Code Warrior?

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

0 件の賞賛
返信
3,664件の閲覧回数
sushilnikam
Contributor III
0 件の賞賛
返信
3,663件の閲覧回数
lalit0611
Contributor II

This is exactly what my doubt was. Thanks Sushil, Tim and David for clearing my doubts :smileyhappy:

0 件の賞賛
返信