IS THERE AN NEED FOR EDUCATION IN USING RISC-V ISA FOR SENSORS AND SOFTWARE REQUIREMENTS WITH THE POSSIBILITY OF NO FIRST ERROR? A TECHNIQUE?
解決済! 解決策の投稿を見る。
Hi,
since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS are very useful, my process may be be a needed one?
Thus, my process may be applicable to many different type of mems as I only used it for a specific 3-axis magnetic MEMS.
John
Which part do you mean for this topic?
Hi,
since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS are very useful, my process may be be a needed one?
Thus, my process may be applicable to many different type of mems as I only used it for a specific 3-axis magnetic MEMS.
John