RISC-V EDUCATION

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RISC-V EDUCATION

跳至解决方案
2,124 次查看
CYBORGJ
Contributor I

IS THERE AN NEED FOR EDUCATION IN USING RISC-V  ISA  FOR SENSORS AND SOFTWARE REQUIREMENTS WITH THE POSSIBILITY OF NO FIRST ERROR? A TECHNIQUE?

0 项奖励
回复
1 解答
2,105 次查看
CYBORGJ
Contributor I

Hi,

since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS  are very useful, my process may be be a needed one?

 

Thus, my process may be applicable to many different type of mems as I only used it for a specific  3-axis magnetic MEMS.

 

John

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,120 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Which part do you mean for this topic?


0 项奖励
回复
2,106 次查看
CYBORGJ
Contributor I

Hi,

since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS  are very useful, my process may be be a needed one?

 

Thus, my process may be applicable to many different type of mems as I only used it for a specific  3-axis magnetic MEMS.

 

John

0 项奖励
回复