Pressure Sensor Choiche

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pressure Sensor Choiche

903 Views
mattiad
Contributor II

Hi,

I wold like to use a pressure sensor for fluidic application which can reach a maximum pressure of 1500kPascal.

Do you have any advice? It should work also with liquid components.

Is the FXTH87 usable with liquid?

Thank you in advance

Mattia

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

820 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Mattia,

 

FXTH871xD is the only pressure sensor family in the current portfolio capable of measure pressure up to 1500 kPa.

 

For all NXP pressure sensor products, any environment other than dry air, will may have some impact on the reliability and lifetime of the product. NXP's silicon pressure sensors are NOT compatible with oil, gas, petrol and can be affected by water or water vapors, or other chemicals.

 

A determination must be made if this impact is acceptable for the application.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply