NTM88 firmware update using SPI interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTM88 firmware update using SPI interface

1,951件の閲覧回数
Markel
Contributor I

Hi,

Is it possible to update the firmware of NXP NTM88 through SPI interface?

Regards,

Markel

0 件の賞賛
返信
4 返答(返信)

1,932件の閲覧回数
Markel
Contributor I

Hi Jozef,

Just to be clear, the answer is the NTM88 firmware can not be updated through SPI interface?

Regards,

Markel

0 件の賞賛
返信

1,917件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Markel,

as I understand it, it is possible to update the firmware through the SPI interface. 

JozefKozon_0-1656935438462.png

With Best Regards,

Jozef

0 件の賞賛
返信

1,912件の閲覧回数
Markel
Contributor I

Hi Jozef,

It does say write memory could be RAM. It does not say write to flash or non-volatile memory. There is no guide or application note that says firmware can be updated using SPI interface. Also, from what I know bootloader needs to support it.

Regards,

Markel

0 件の賞賛
返信

1,947件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Markel,

according to UM11227, the NTM88 supports client SPI for host access to internal peripherals, registers, and memory. 

JozefKozon_0-1656673402543.png

There is an AN12523 Firmware versus Library model applications, please download it from here. Other application notes can be also downloaded from the same link.

JozefKozon_1-1656673763947.png

With Best Regards,

Jozef

0 件の賞賛
返信