JozefKozon
		
			JozefKozon
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Markel,
as I understand it, it is possible to update the firmware through the SPI interface.
With Best Regards,
Jozef
Hi Jozef,
It does say write memory could be RAM. It does not say write to flash or non-volatile memory. There is no guide or application note that says firmware can be updated using SPI interface. Also, from what I know bootloader needs to support it.
Regards,
Markel
 JozefKozon
		
			JozefKozon
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Markel,
according to UM11227, the NTM88 supports client SPI for host access to internal peripherals, registers, and memory.
There is an AN12523 Firmware versus Library model applications, please download it from here. Other application notes can be also downloaded from the same link.
With Best Regards,
Jozef