NTM88 firmware update using SPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTM88 firmware update using SPI interface

2,016 Views
Markel
Contributor I

Hi,

Is it possible to update the firmware of NXP NTM88 through SPI interface?

Regards,

Markel

0 Kudos
Reply
4 Replies

1,997 Views
Markel
Contributor I

Hi Jozef,

Just to be clear, the answer is the NTM88 firmware can not be updated through SPI interface?

Regards,

Markel

0 Kudos
Reply

1,982 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Markel,

as I understand it, it is possible to update the firmware through the SPI interface. 

JozefKozon_0-1656935438462.png

With Best Regards,

Jozef

0 Kudos
Reply

1,977 Views
Markel
Contributor I

Hi Jozef,

It does say write memory could be RAM. It does not say write to flash or non-volatile memory. There is no guide or application note that says firmware can be updated using SPI interface. Also, from what I know bootloader needs to support it.

Regards,

Markel

0 Kudos
Reply

2,012 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Markel,

according to UM11227, the NTM88 supports client SPI for host access to internal peripherals, registers, and memory. 

JozefKozon_0-1656673402543.png

There is an AN12523 Firmware versus Library model applications, please download it from here. Other application notes can be also downloaded from the same link.

JozefKozon_1-1656673763947.png

With Best Regards,

Jozef

0 Kudos
Reply