Minimum Operating Pressure for MPXM2102AS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Minimum Operating Pressure for MPXM2102AS

1,894 次查看
jeffreyheadrick
Contributor I

The data sheet for the MPX2102 series sensors states the minimum pressure for the MPX2102A sensor is 20 kPa.  Does this extend to all absolute pressure sensors in the series or just that particular package?  We have an application with size constraints (favoring the MPXM2102AS); however, requires functionality near 5 kPa absolute.  Please advise.

标签 (1)
0 项奖励
回复
2 回复数

1,594 次查看
Emilien38
Contributor I

Hello,

We used in our project the obsolete sensor :MPX2100A (LINK).

It's not possible to buy it, so an alternative seems the MPX2102A (LINK).

I see one difference about the minimum operating pressure : 0kPa for the MPX2100A  and 20kPa for MPX2102A . are there other difference between them? The internal electronic of the sensor is different, no error on the datasheet?

Thank you, Emilien

0 项奖励
回复

1,758 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jeffrey,

As you can see on this website, the minimum operating pressure of our absolute pressure sensors is either 15 kPa or 20 kPa.

 

For lower pressure, we can offer the MPXV6115V gauge vacuum sensor in SOP package.

Best regards,

Tomas

0 项奖励
回复