Minimum Operating Pressure for MPXM2102AS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum Operating Pressure for MPXM2102AS

1,840 Views
jeffreyheadrick
Contributor I

The data sheet for the MPX2102 series sensors states the minimum pressure for the MPX2102A sensor is 20 kPa.  Does this extend to all absolute pressure sensors in the series or just that particular package?  We have an application with size constraints (favoring the MPXM2102AS); however, requires functionality near 5 kPa absolute.  Please advise.

Labels (1)
0 Kudos
Reply
2 Replies

1,540 Views
Emilien38
Contributor I

Hello,

We used in our project the obsolete sensor :MPX2100A (LINK).

It's not possible to buy it, so an alternative seems the MPX2102A (LINK).

I see one difference about the minimum operating pressure : 0kPa for the MPX2100A  and 20kPa for MPX2102A . are there other difference between them? The internal electronic of the sensor is different, no error on the datasheet?

Thank you, Emilien

0 Kudos
Reply

1,704 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jeffrey,

As you can see on this website, the minimum operating pressure of our absolute pressure sensors is either 15 kPa or 20 kPa.

 

For lower pressure, we can offer the MPXV6115V gauge vacuum sensor in SOP package.

Best regards,

Tomas

0 Kudos
Reply