MPXV7002 Reference Pressure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPXV7002 Reference Pressure

1,182 次查看
pambrose
Contributor I

Hello,

I have a quick question regarding the single port variants of the MPXV7002 pressure sensors. I just wanted to confirm that these single port models are referencing port 1 pressure to the sensor's ambient pressure, and not an internal vacuum. It seems that the latter would exceed the device's maximum pressure rating of 75 kPa, but I just wanted to make sure. Thank you,

Austin

0 项奖励
回复
2 回复数

1,175 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

The single ported versions of the MPXV7002 are all Gauge Pressure sensors, which means that the reference pressure is open to local atmospheric pressure.

The reference pressure ‘port’ on Gauge sensors is an open hole in the bottom of the sensor, while port ‘P1’ is the one used to attach to the hose to measure the pressure.

You need to make sure that the differential pressure between port P1 and reference pressure is never higher than 75kPa.

Regards,

Jose

1,172 次查看
pambrose
Contributor I

Hi Reyes,

Perfect. Than you for clarifying and for your quick reply. Cheers,

Austin

0 项奖励
回复