MPXV7002 Reference Pressure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXV7002 Reference Pressure

1,181 Views
pambrose
Contributor I

Hello,

I have a quick question regarding the single port variants of the MPXV7002 pressure sensors. I just wanted to confirm that these single port models are referencing port 1 pressure to the sensor's ambient pressure, and not an internal vacuum. It seems that the latter would exceed the device's maximum pressure rating of 75 kPa, but I just wanted to make sure. Thank you,

Austin

0 Kudos
Reply
2 Replies

1,174 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

The single ported versions of the MPXV7002 are all Gauge Pressure sensors, which means that the reference pressure is open to local atmospheric pressure.

The reference pressure ‘port’ on Gauge sensors is an open hole in the bottom of the sensor, while port ‘P1’ is the one used to attach to the hose to measure the pressure.

You need to make sure that the differential pressure between port P1 and reference pressure is never higher than 75kPa.

Regards,

Jose

1,171 Views
pambrose
Contributor I

Hi Reyes,

Perfect. Than you for clarifying and for your quick reply. Cheers,

Austin

0 Kudos
Reply