Hi Prathamesh Dhanpalwar,
Package used in the MPXV5050GP is a SOP-8 with a case no. 1369-01, package dimensions of this device can be found here.
As stated in Document DOC-97353, the difference between style 1 and style 2 in the package dimensions is due to the two main families of pressure sensors Freescale offers.
Style 1 is usually applicable for all MPXx10, MPXx53 and MPXx2000-series SOP Type package pressure sensors featuring differential outputs.
Style 2 is applicable for all MPXx4000-series, MPXx5000-series, MPXx6000-series, MPXx7000-series integrated devices in surface mount packages featuring single ended outputs.
So for the case of the MPXV5050GP, case no. 1369-01, you should use Style 2:
Pin 1: N/C
Pin 2: Vs
Pin3: GND
Pin 4: Vout
Pin 5: N/C
Pin 6: N/C
Pin 7: N/C
Pin 8: N/C
Additionally, you can find a 3D Step design for this package here.
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------