MPX2100D: What is the rated leak rate?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPX2100D: What is the rated leak rate?

620 Views
stevenj8
Contributor II

See title.

Labels (1)
0 Kudos
1 Reply

420 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Steve Clark,

Leakage is an unspecified and therefore not guaranteed performance characteristic of our devices. However, Freescale does perform a 100% leakage test on all ported devices after assembly. The intent/extent of FSL's test capabilities is as a manufacturing quality tool/gauge to identify gross leakers (devices outside the leak test limits), NOT to quantify leakage as a cc/sec performance characteristic.

An additional recommendation when using ported pressure sensors, I would recommend to use hose clamps to helping prevent leakage and loosening, hose clamps provide a stronger connection to the sensor port. Clamps that are recommended for use in applications as described are the Oetiker Two-Ear Clamp, and the Oetiker One-Ear, and Special Clamp from Newage Industries.

AN1513: Mounting Techniques and Plumping Options of MPX Series Pressure Sensors

http://www.freescale.com/files/sensors/doc/app_note/AN1513.pdf


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos