MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

1,117件の閲覧回数
CVi
Contributor I

Hi,

I wander if is it possible to hardware-detect which of the two MPX5700DP / MPX5500DP sensors is mounted on the board.

Can I use the V1, V2 and Vex pins with some circuitry between the sensor and the MCU to detect which sensor is connected? If yes, how? What type of signals are them?

I found in other questions (1, 2, 3) that those pins must be leave not connected.

But is there any possibility to use them for this scope, please?

Thank you in advance.

 

Bye,

Clem

0 件の賞賛
返信
2 返答(返信)

1,088件の閲覧回数
CVi
Contributor I

Ok, Tomas, thank you anyway.

Best regards,

Clemente

0 件の賞賛
返信

1,097件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Clemente,

I am afraid there is no way to use these pins for this purpose and I cannot think of any other suitable possibility to achieve that, unfortunately.

Best regards,

Tomas

0 件の賞賛
返信