MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

1,193 次查看
CVi
Contributor I

Hi,

I wander if is it possible to hardware-detect which of the two MPX5700DP / MPX5500DP sensors is mounted on the board.

Can I use the V1, V2 and Vex pins with some circuitry between the sensor and the MCU to detect which sensor is connected? If yes, how? What type of signals are them?

I found in other questions (1, 2, 3) that those pins must be leave not connected.

But is there any possibility to use them for this scope, please?

Thank you in advance.

 

Bye,

Clem

0 项奖励
回复
2 回复数

1,164 次查看
CVi
Contributor I

Ok, Tomas, thank you anyway.

Best regards,

Clemente

0 项奖励
回复

1,173 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Clemente,

I am afraid there is no way to use these pins for this purpose and I cannot think of any other suitable possibility to achieve that, unfortunately.

Best regards,

Tomas

0 项奖励
回复