MPL3115A2 support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL3115A2 support

1,078 Views
phani_kagithapu
Contributor I

We are using Part no : MPL3115A2  absolute pressure in one of our product .

 

Please confirm , whether is it appropriate to read the temperature value  from MPL3115A2 continuously, where the sensor is closed under air sealed box (no exposure with ambient air).

 

Regards,

Phani.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

822 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Phani,

Yes, you can use the MPL3115A2 embedded temperature sensor to read the temperature value continuously, although since the sensor is closed under air sealed box (no exposure with ambient air), you will not be reading the ambient temperature but the temperature inside the MPL3115A2.

Temperature reading are taken from the internal ADC and it would read the internal die temperature which is used for the pressure compensation of the pressure output more than to be used as an “ambient temperature sensor” so it is not recommended to use it that way if the temperature accuracy is an important feature of your application.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply