MAG3110 as current detector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAG3110 as current detector

1,012 Views
simonecerri
Contributor I

Hi, I wonder if MAG3110 could be suitable to detect 110/220V power line buried in the wall/ground? Does anyone have experience about it? Thank you

Labels (1)
0 Kudos
Reply
1 Reply

826 Views
david_diaz
NXP Employee
NXP Employee

Hello Simone,

I know that the NXP Magnetometer, the MAG3110, has been tested to detect presence of AC voltage due to the electromagnetic field generated, however, test results are very variable.

It will depend on where you need to measure the voltage, for example, using the MAG3110 you can easily detect (after proper calibration) the presence of AC voltage directly measuring in the AC cables, but it is very hard to detect presence of it through the walls.

So, as a conclusion and to be honest with you, I would say that it is possible to detect the presence of AC voltage using a Magnetometer, but it is not reliable.

I hope this information helps.

David

0 Kudos
Reply