MPL3115A2-Soldering Recommendations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL3115A2-Soldering Recommendations

Jump to solution
2,012 Views
haiyu
Contributor I

Hello,

       I am trying to use the MPL3115A2 sensor to measure temperature and pressure,so I need soldering recommendations for the MPL3115A2 sensor.Is there a datasheet about soldering?

       Who can send it to me?thanks!

Labels (1)
1 Solution
1,669 Views
reyes
NXP TechSupport
NXP TechSupport

Hi hai yu,

You can find useful information about the soldering recommendations for LGA packages in the application note AN3484

Although this document is not designed for the MPL3115A2, is related to the same or very similar LGA package, so you can use this document as a reference for the soldering recommendations.

You can also check some specific recommendation for pressure sensors in the Application note AN3150.

I hope this helps.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,670 Views
reyes
NXP TechSupport
NXP TechSupport

Hi hai yu,

You can find useful information about the soldering recommendations for LGA packages in the application note AN3484

Although this document is not designed for the MPL3115A2, is related to the same or very similar LGA package, so you can use this document as a reference for the soldering recommendations.

You can also check some specific recommendation for pressure sensors in the Application note AN3150.

I hope this helps.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,669 Views
haiyu
Contributor I

Hi Jose Reyes,

Thank you for the answer.It is useful for me. I have referred to the note AN3150​.There are some specific recommendations for pressure sensors.The board was soldered and worked normally.Thanks!