MMA8652FC 8 bits Offset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA8652FC 8 bits Offset

1,742 次查看
sérgioneves
Contributor I

Hello everyone,

I follow the project "MMA8652FC - Bare metal example project", link

But if I want to use the sensor configured to use 8 bits, how do I calculate the offset values?

I get the Xout_8_bit, Yout_8_bit, Zout_8_bit. And I know the sensitivity:

SENSITIVITY_2G_8bits        64

SENSITIVITY_4G_8bits        32

SENSITIVITY_8G_8bits        16

So how to get:

X_offset_2G_8_bit = ?

Y_offset_2G_8_bit = ?

Z_offset_2G_8_bit = ?

X_offset_4G_8_bit = ?

Y_offset_4G_8_bit = ?

Z_offset_4G_8_bit = ?

X_offset_8G_8_bit = ?

Y_offset_8G_8_bit = ?

Z_offset_8G_8_bit = ?

Thanks.

Regards,

Sérgio

标签 (1)
0 项奖励
回复
2 回复数

1,483 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sérgio,

SENSITIVITY_2G_8bits        64

SENSITIVITY_4G_8bits        32

SENSITIVITY_8G_8bits        16

 

±2g:

X_offset_2G_8_bit = Xout_8_bit * 8 * (-1);   

Y_offset_2G_8_bit = Yout_8_bit * 8 * (-1);   

Z_offset_2G_8_bit = (Zout_8_bit - SENSITIVITY_2G_8bits) * 8 * (-1);

 

±4g:

X_offset_4G_8_bit = Xout_8_bit * 16 * (-1);   

Y_offset_4G_8_bit = Yout_8_bit * 16 * (-1);   

Z_offset_4G_8_bit = (Zout_8_bit - SENSITIVITY_4G_8bits) * 16 * (-1);

 

±8g:

X_offset_8G_8_bit = Xout_8_bit * 32 * (-1);   

Y_offset_8G_8_bit = Yout_8_bit * 32 * (-1);   

Z_offset_8G_8_bit = (Zout_8_bit - SENSITIVITY_8G_8bits) * 32 * (-1);

Best regards,

Tomas

0 项奖励
回复

1,483 次查看
sérgioneves
Contributor I

Hello Tomas,

Thanks for all the help.

Regards,

Sérgio

0 项奖励
回复