MM9Z1_638 XTAL no signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1_638 XTAL no signal

Jump to solution
1,579 Views
a852013777
Contributor III

Hi Nxp Partner

We try to write firware code when we get our first version senior board (installs MM9Z1_638).

We found EXTAL& XTAL is oscillation signal and We also check all the voltage pin of MM9Z1_638 (VDDA,VDDX,VDDH,VDD2D,LTO ,RESET) is within the spec's requirement.Do you have any suggestion to check why EXTAL& XTAL no signal?

 

Br,

Mike Liang

0 Kudos
Reply
1 Solution
1,572 Views
a852013777
Contributor III

hi jozef

Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?

"without  extal signal"can we wirte firmware to mm9z1_638 now ?

 

Br 

Mike liang 

View solution in original post

0 Kudos
Reply
3 Replies
1,576 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mike,

please check the OSCE bit in the CPMUOSC register. It should be set to 1 to see an external wave on the EXTAL pin.

JozefKozon_0-1663838436469.png

JozefKozon_1-1663838463181.png

With Best Regards,

Jozef

0 Kudos
Reply
1,573 Views
a852013777
Contributor III

hi jozef

Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?

"without  extal signal"can we wirte firmware to mm9z1_638 now ?

 

Br 

Mike liang 

0 Kudos
Reply
1,555 Views
a852013777
Contributor III

hi jozef

We add 470nf on two reset pin. We can write firmware. thanks 

 

Br,

Mike Liang