Log accelerometer data and barometer data to SD card with the FRDM-FXS-MULT2-B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Log accelerometer data and barometer data to SD card with the FRDM-FXS-MULT2-B

ソリューションへジャンプ
1,920件の閲覧回数
gislibergursigu
Contributor I

Hi all,

Not sure if this is the right place, but i just received the FRDM-FXS-MULT2-B and the FRDM-K64F. I'm having a hard time finding any information about how to log data to an SD card.

Basicly what I want to be able to do is to log the X,Y,Z axis from the FXLS8471Q and pressure and temperature to a SD card while the device is running on battery and then beeing able to retrive the data from the SD card for further analyzis.

Does anybody hold any information about weather this is possible or not? And if there is any code available that is capable of doing this?

Best regards,

Gisli Bergur

ラベル(2)
0 件の賞賛
返信
1 解決策
1,268件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Gisli,

I would recommend taking a closer look at the following tutorials/projects:

Tutorial: Data Logger with the FRDM-K64F Board:

http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/

FatFs + SDHC data logger with KSDK in Kinetis Design Studio:

https://community.freescale.com/docs/DOC-105852

FRDM K64F Data Logger using FatFs with KSDK 1.2.0:

http://centaurian.co.uk/2015/07/15/frdm-k64f-data-logger-using-fatfs-with-ksdk-1-2-0/

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,269件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Gisli,

I would recommend taking a closer look at the following tutorials/projects:

Tutorial: Data Logger with the FRDM-K64F Board:

http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/

FatFs + SDHC data logger with KSDK in Kinetis Design Studio:

https://community.freescale.com/docs/DOC-105852

FRDM K64F Data Logger using FatFs with KSDK 1.2.0:

http://centaurian.co.uk/2015/07/15/frdm-k64f-data-logger-using-fatfs-with-ksdk-1-2-0/

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信