Hi all,
Not sure if this is the right place, but i just received the FRDM-FXS-MULT2-B and the FRDM-K64F. I'm having a hard time finding any information about how to log data to an SD card.
Basicly what I want to be able to do is to log the X,Y,Z axis from the FXLS8471Q and pressure and temperature to a SD card while the device is running on battery and then beeing able to retrive the data from the SD card for further analyzis.
Does anybody hold any information about weather this is possible or not? And if there is any code available that is capable of doing this?
Best regards,
Gisli Bergur
Solved! Go to Solution.
Hi Gisli,
I would recommend taking a closer look at the following tutorials/projects:
Tutorial: Data Logger with the FRDM-K64F Board:
http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/
FatFs + SDHC data logger with KSDK in Kinetis Design Studio:
https://community.freescale.com/docs/DOC-105852
FRDM K64F Data Logger using FatFs with KSDK 1.2.0:
http://centaurian.co.uk/2015/07/15/frdm-k64f-data-logger-using-fatfs-with-ksdk-1-2-0/
I hope it helps.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Hi Gisli,
I would recommend taking a closer look at the following tutorials/projects:
Tutorial: Data Logger with the FRDM-K64F Board:
http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/
FatFs + SDHC data logger with KSDK in Kinetis Design Studio:
https://community.freescale.com/docs/DOC-105852
FRDM K64F Data Logger using FatFs with KSDK 1.2.0:
http://centaurian.co.uk/2015/07/15/frdm-k64f-data-logger-using-fatfs-with-ksdk-1-2-0/
I hope it helps.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.