LM75BTP exposed pad connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LM75BTP exposed pad connection

ソリューションへジャンプ
1,210件の閲覧回数
fdm
Contributor IV

Hi,

LM75BTP temperature sensor in SOT1069-2 / HWSON8 package has the exposed center pad.

Does this pad have an internal connection to GND (or any other pin) or it is NC and may be externally connected to any net as convenient?

BR,
   Denis

0 件の賞賛
返信
1 解決策
920件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Denis,

Thanks for your interest in the LM75BTP!

The exposed par is internally connected to GND, so leave it either unconnected or connect it to GND.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

1 返信
921件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Denis,

Thanks for your interest in the LM75BTP!

The exposed par is internally connected to GND, so leave it either unconnected or connect it to GND.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.