I'm using MMA8451 - Can I permanently write settings to the sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm using MMA8451 - Can I permanently write settings to the sensor

ソリューションへジャンプ
1,537件の閲覧回数
davidgroff
Contributor II

I am using an Arduino Uno to write configuration settings to the MMA8451.  I have set it up to detect freefall and set interrupt pin 1.  I want to know if I can save these settings in non-volatile memory of the chip so that I don't need to re-write these to the chip every time power is reset?:

Thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,411件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

Unfortunately not. The non-volatile memory is not user accessible. The only way is to write the register configuration every time after powering up from your Atmega328 MCU.


Let me know if you have any other questions.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,412件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

Unfortunately not. The non-volatile memory is not user accessible. The only way is to write the register configuration every time after powering up from your Atmega328 MCU.


Let me know if you have any other questions.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信