How to test MPL3115A2 with sensor fusion toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test MPL3115A2 with sensor fusion toolbox

ソリューションへジャンプ
1,863件の閲覧回数
chiranjeevikinn
Contributor III

Hi,

I want to test the MPL3115A2 sensor. I am using the FRDM-KL25Z and FRDM-FXS-MULTI on which I can see the MPL3115A2 . I am not seeing any option to see how Altimeter works in sensor fusion toolbox.

It would a great help if someone can suggest me how I can test the it.

 

Thanks,

Chiranjeevi

ラベル(1)
1 解決策
1,681件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Chiranjeevi,

Assuming your KL25Z binary was built assuming that the MPL3115A2 is present (and those for the MULTI/MULTI-B are), you should see an "Altimeter" tab like that shown below.  It shows computed altitude and measured temperature vs time.  Not terribly exciting, but it at least gives you a starting point.

Mike

AltimeterTab.png

元の投稿で解決策を見る

2 返答(返信)
1,682件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Chiranjeevi,

Assuming your KL25Z binary was built assuming that the MPL3115A2 is present (and those for the MULTI/MULTI-B are), you should see an "Altimeter" tab like that shown below.  It shows computed altitude and measured temperature vs time.  Not terribly exciting, but it at least gives you a starting point.

Mike

AltimeterTab.png

1,681件の閲覧回数
chiranjeevikinn
Contributor III

Hi Mike,

Thank you very much. It works for me.

Regards,

Chiranjeevi

0 件の賞賛
返信