How to test MPL3115A2 with sensor fusion toolbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to test MPL3115A2 with sensor fusion toolbox

跳至解决方案
1,823 次查看
chiranjeevikinn
Contributor III

Hi,

I want to test the MPL3115A2 sensor. I am using the FRDM-KL25Z and FRDM-FXS-MULTI on which I can see the MPL3115A2 . I am not seeing any option to see how Altimeter works in sensor fusion toolbox.

It would a great help if someone can suggest me how I can test the it.

 

Thanks,

Chiranjeevi

标签 (1)
1 解答
1,641 次查看
michaelestanley
NXP Employee
NXP Employee

Chiranjeevi,

Assuming your KL25Z binary was built assuming that the MPL3115A2 is present (and those for the MULTI/MULTI-B are), you should see an "Altimeter" tab like that shown below.  It shows computed altitude and measured temperature vs time.  Not terribly exciting, but it at least gives you a starting point.

Mike

AltimeterTab.png

在原帖中查看解决方案

2 回复数
1,642 次查看
michaelestanley
NXP Employee
NXP Employee

Chiranjeevi,

Assuming your KL25Z binary was built assuming that the MPL3115A2 is present (and those for the MULTI/MULTI-B are), you should see an "Altimeter" tab like that shown below.  It shows computed altitude and measured temperature vs time.  Not terribly exciting, but it at least gives you a starting point.

Mike

AltimeterTab.png

1,641 次查看
chiranjeevikinn
Contributor III

Hi Mike,

Thank you very much. It works for me.

Regards,

Chiranjeevi

0 项奖励
回复